URL:
/zh-cn/go/akb/201500064/1
One controller for Logic and Motion (FAST)
Function extension:Due to the new Lenze FAST license model, it is possible to use the same…
URL:
/zh-cn/go/akb/201500061/1
CFC Editor: New functions
Function extension:
The CFC Editor has been enhanced by the following functions:
Grouping elementsIn…
URL:
/zh-cn/go/akb/201500045/1
FAST Motion: Libraries
Function extension:
For FAST Motion, the following Lenze libraries have been added to the Library Repository…
URL:
/zh-cn/go/akb/201500046/1
FAST Motion: Cam Editor
Function extension:
The new Cam Editor can be used to display, create and edit FAST Motion cam and tappet…
URL:
/zh-cn/go/akb/201500047/1
FAST Motion: Axis groups
Function extension:
Kinematics is used to describe the mechanical structure of robots. The robot axes are…
URL:
/zh-cn/go/akb/201500048/1
FAST Motion: Reconstruction of reference information
Function extension:
Via the FAST Motion axis parameter with subindex 81 (=…
URL:
/zh-cn/go/akb/201500049/1
FAST Motion: Parameterising the Motion
Function extension:
When adding a Motion axis to the device tree, a parameter structure with…
URL:
/zh-cn/go/akb/201500060/1
Visualisation: Simplified use of frames
Function extension:
By entering the data type or the instance name, the referenced…
URL:
/zh-cn/go/akb/201500062/1
Structured text: IEC-extending operators
Function extension:
In structured text, the following operators can be used in an IF…
URL:
/zh-cn/go/akb/201500004/1
Hiperface SinCos absolute value encoder: Functionality of monitoring modes has been extended and improved (from V1.7.5)
Function…
URL:
/zh-cn/go/akb/201500059/1
ApplicationTemplate – PackML standard: Automatic insertion of a user mode
Function extension:
In the ApplicationTemplate…
URL:
/zh-cn/go/akb/201500053/1
L_EATP_ApplicationTemplate library: L_EATP_UserCoupling function block
Function extension:
The L_EATP_UserCoupling function block is…
URL:
/zh-cn/go/akb/201500054/1
L_EATP_ApplicationTemplate library: New baseChannel methods
Function extension:
The following methods have been added to the…
URL:
/zh-cn/go/akb/201500056/1
L_EATP_ApplicationTemplate library: Integration of ISA 88 command structure
Function extension:
In the ApplicationTemplate PackML…