URL:
/pt-br/go/akb/201100922/1
New codes for the EMF2178IB AIF module (CANopen)
Function description
The following four codes have been added to the PLC target system…
URL:
/pt-br/go/akb/201100901/1
Extension of the absolute value encoder selection
Function description
The following Sick-Stegmann absolute value encoders are supported…
URL:
/pt-br/go/akb/201010850/1
Loading the default setting for the OPERATING SYSTEM and processing the code initialisation list for the application software with C0002=2…
URL:
/pt-br/go/akb/201013240/1
Free CAN-PDO: Monitoring of received CAN telegrams removed (as of ECS OPERATING SYSTEM V8.3, SPLC V8.0)
Function extension:
The…
URL:
/pt-br/go/akb/201010922/1
Extension of the L_ParRead() and L_ParWrite() functions
Function description
From the LenzeDrive0203.lib library onwards the…
URL:
/pt-br/go/akb/201010916/1
Fail-QSP fault response added to brake relay monitoring (C0602=4) (as of OPERATING SYSTEM V8.3)
Function extension:
The fault…
URL:
/pt-br/go/akb/201014938/1
L_Counter FB - additional comparison operations
Function extension:
Function extension of the comparison operation
Included in…
URL:
/pt-br/go/akb/201006032/1
Homing - evaluation of the hardware limits
Function extension:
In the Homing operating mode, homing can be started from an…
URL:
/pt-br/go/akb/201006028/1
Homing: level-controlled start of homing
Function extension:
So far homing has not been started if the bHomeStartStop control…
URL:
/pt-br/go/akb/201006030/1
ManualJog - additional parameters for second speed have been removed
Function extension:
In addition to the time to be set,…
URL:
/pt-br/go/akb/201006031/1
ManualJog effect of the deceleration override also when stopping
Function extension:
When the acceleration override was…
URL:
/pt-br/go/akb/201005119/1
Software limit position recognition - software limit position approached
Function extension
The information that software limit positions…
URL:
/pt-br/go/akb/201005118/1
Support of new fieldbus modules
Function extension
The following fieldbus modules are supported:
PROFIBUS (from V02.00)EtherCat (from…
URL:
/pt-br/go/akb/201014119/1
Extended diagnostics options
Function description The following codes have been included in SM301 V1.4 in order to facilitate the safety…