URL:
/fr-be/go/akb/201900399/1
New parameters
Function extension: The Lenze controller has the following new parameters: Life-diagnosis: operating time…
URL:
/fr-be/go/akb/201900398/1
Device search for controller backplane bus
Function extension: The Lenze controller supports device search on the controller backplane…
URL:
/fr-be/go/akb/201900397/1
Parallel parameter set download
Function extension:When the EtherCAT bus is started, the Lenze controller loads the configured…
URL:
/fr-be/go/akb/201900414/1
MMC configuration files for optional EtherCAT devices in the PLC project
Function extension: The configuration files required for the…
URL:
/fr-be/go/akb/201900406/1
New source code navigation commands
Function extension: In the dialog 'Customize' (menu 'Tools'>'Customize') two new commands are…
URL:
/fr-be/go/akb/201900394/1
Support of a new touch controller for Lenze monitor panels
Function extension: As part of series maintenance, the TSHARC touch…
URL:
/fr-be/go/akb/201900404/1
CFC Editor: Multiple insertion of the same operator
Function extension: The same operator can be inserted several times in the CFC…
URL:
/fr-be/go/akb/201900403/1
ST editor improvements
Function extension: The ST editor has been improved as follows:Identical symbols are highlightedIf a…
URL:
/fr-be/go/akb/201900402/1
New data type __VECTOR
Function extension: A vector data type is a floating point array with a maximum of 8 elements. The…
URL:
/fr-be/go/akb/201900400/1
Improvements of the input help
Function extension: The following points of the input help have been improved:If a component…
URL:
/fr-be/go/akb/201900396/1
Support of the new Lenze controllers c520 and c750
Function extension: The PLC Designer supports the new Lenze controllers c520 and…
URL:
/fr-be/go/akb/201900395/1
i550: Parameter set download if required
Function extension: When the boot application is started in the Lenze controller (e.g. when…
URL:
/fr-be/go/akb/201900393/1
Support of the new LAN controller
Function extension: The new firmware V3.18 and the corresponding software Backup&Restore V3.18…