URL:
/fr-be/go/akb/201010922/1
Extension of the L_ParRead() and L_ParWrite() functions
Function description
From the LenzeDrive0203.lib library onwards the…
URL:
/fr-be/go/akb/201010916/1
Fail-QSP fault response added to brake relay monitoring (C0602=4) (as of OPERATING SYSTEM V8.3)
Function extension:
The fault…
URL:
/fr-be/go/akb/201014938/1
L_Counter FB - additional comparison operations
Function extension:
Function extension of the comparison operation
Included in…
URL:
/fr-be/go/akb/201006032/1
Homing - evaluation of the hardware limits
Function extension:
In the Homing operating mode, homing can be started from an…
URL:
/fr-be/go/akb/201006028/1
Homing: level-controlled start of homing
Function extension:
So far homing has not been started if the bHomeStartStop control…
URL:
/fr-be/go/akb/201006030/1
ManualJog - additional parameters for second speed have been removed
Function extension:
In addition to the time to be set,…
URL:
/fr-be/go/akb/201006031/1
ManualJog effect of the deceleration override also when stopping
Function extension:
When the acceleration override was…
URL:
/fr-be/go/akb/201005119/1
Software limit position recognition - software limit position approached
Function extension
The information that software limit positions…
URL:
/fr-be/go/akb/201005118/1
Support of new fieldbus modules
Function extension
The following fieldbus modules are supported:
PROFIBUS (from V02.00)EtherCat (from…
URL:
/fr-be/go/akb/201014119/1
Extended diagnostics options
Function description The following codes have been included in SM301 V1.4 in order to facilitate the safety…
URL:
/fr-be/go/akb/201014118/1
Plausibility check
Function description The default value of the 'OMS: Motion function' was changed from 'SLS1' to 'Free traversing'.…
URL:
/fr-be/go/akb/201014115/1
Ramp monitoring with SS1 / SS2
Function description When SS1 or SS2 has been activated the SM301 has up to now only checked by at the end…
URL:
/fr-be/go/akb/201014113/1
Safely limited increment
Function description The function is an extension of the safe tip mode function.
After pressing the enable…
URL:
/fr-be/go/akb/201014112/1
Resolver support (single encoder concept)
Function description Up to now, a sine/cosine encoder or a resolver in combination with another…
URL:
/fr-be/go/akb/201013874/1
Suppression of Profibus DP-V1 diagnostic messages by means of C13887 and C14887 (from V1.20)
New function in:
Communication module…