URL:
/ru-ru/go/akb/20023520/1
Fault indication Pr5 or fault number 79
Question:
Pr5 fault indication or fault number 79, meaning and procedure?
Answer:…
URL:
/ru-ru/go/akb/20010010/1
Absolute value encoders with Hiperface, operation possible with 9300 and ECS ? (single turn: SRS50, SRS64, SCS60, SCS70, SKS36, multi…
URL:
/ru-ru/go/akb/20023571/1
No touch probe detection
Question:
Why is no touch probe signal detected via the digital input X5/E4 or via a zero pulse of the…
URL:
/ru-ru/go/akb/20024116/1
Quickstop when usage of the internal PID controller
Question: How can the quickstop function be used when the internal PID controller…
URL:
/ru-ru/go/akb/20023926/1
Parallel operation of two motors at 9300 servo inverter
Question:
Is it possible to operate two motors parallel at a 9300 servo, and…
URL:
/ru-ru/go/akb/20024059/1
COM ports, which ones are supported by GDC?
Question:
Which COM ports are supported by the Lenze parameter setting software GDC…
URL:
/ru-ru/go/akb/20024077/1
I²xt function of the 8200 vector / motec
Question:
How are parameters set to the internal motor temperature monitoring (I²x t…
URL:
/ru-ru/go/akb/20024186/1
Register mark or cylinder mark distance, standardisation
Question:
Which value does the standardisation of the following code digits…
URL:
/ru-ru/go/akb/20024298/1
Current controller adjustment, setting the current controller parameters (C0075, C0076), 9300 and ECS
Question:
Under which…
URL:
/ru-ru/go/akb/20024333/1
Text panels, input of special characters and umlauts
Question:
How can special characters or umlauts are entered in text panels H…
URL:
/ru-ru/go/akb/20024334/1
Detection of task run times for further calculations in the PLC
Question:
How can the run time of the current task be detected?…
URL:
/ru-ru/go/akb/20024346/1
DFSET stretch factor and gearbox factor, correct order
Question:
What has to be considered for the use of stretch factor and gearbox…
URL:
/ru-ru/go/akb/20011608/1
Synchronous motor applied to frequency inverter
Question:
Can a synchronous motor (e. g. SDSGS synchronous servomotor) be applied to…
URL:
/ru-ru/go/akb/20011602/1
Armature chokes, typical temperature during operation of armature chokes
Question:
Which typical surface temperatures are normal /…