URL:
/ru-ru/go/akb/201006030/1
ManualJog - additional parameters for second speed have been removed
Function extension:
In addition to the time to be set,…
URL:
/ru-ru/go/akb/201006031/1
ManualJog effect of the deceleration override also when stopping
Function extension:
When the acceleration override was…
URL:
/ru-ru/go/akb/201005119/1
Software limit position recognition - software limit position approached
Function extension
The information that software limit positions…
URL:
/ru-ru/go/akb/201005118/1
Support of new fieldbus modules
Function extension
The following fieldbus modules are supported:
PROFIBUS (from V02.00)EtherCat (from…
URL:
/ru-ru/go/akb/201014119/1
Extended diagnostics options
Function description The following codes have been included in SM301 V1.4 in order to facilitate the safety…
URL:
/ru-ru/go/akb/201014118/1
Plausibility check
Function description The default value of the 'OMS: Motion function' was changed from 'SLS1' to 'Free traversing'.…
URL:
/ru-ru/go/akb/201014115/1
Ramp monitoring with SS1 / SS2
Function description When SS1 or SS2 has been activated the SM301 has up to now only checked by at the end…
URL:
/ru-ru/go/akb/201014113/1
Safely limited increment
Function description The function is an extension of the safe tip mode function.
After pressing the enable…
URL:
/ru-ru/go/akb/201014112/1
Resolver support (single encoder concept)
Function description Up to now, a sine/cosine encoder or a resolver in combination with another…
URL:
/ru-ru/go/akb/201013874/1
Suppression of Profibus DP-V1 diagnostic messages by means of C13887 and C14887 (from V1.20)
New function in:
Communication module…
URL:
/ru-ru/go/akb/201012448/1
Setting of memory modules which are applied in real plants later (from V8.1 onwards)
Function description
It is now possible to prepare…
URL:
/ru-ru/go/akb/201009924/1
Progress bar for C0002 commands (from V8.0 onwards)
Functional description
In the Engineer from V2.12, commands which can be activated…
URL:
/ru-ru/go/akb/201009928/1
Extension of the torque interface (from V8.0 onwards)
Functional description
The LS_MotorInterface system block has been extended by the…
URL:
/ru-ru/go/akb/201009930/1
Input for resetting the following error (from V8.0 onwards)
Functional description
At the LS_Feedback system block, the…