URL:
/ru-ru/go/akb/202400426/1
Support of UTF-8 for data type STRING
Function extension:UTF8 is a more widely used byte-oriented encoding format for Unicode…
URL:
/ru-ru/go/akb/202400421/1
Multi Client (read only mode)
Function-extension:With PLC Designer V4, several PLC
Designer clients can log in to the same controller.…
URL:
/ru-ru/go/akb/202400424/1
Constant generic variable (VAR_GENERIC CONSTANT)
Function-extension:A generic constant is a variable in the declaration…
URL:
/ru-ru/go/akb/202300409/1
L_MC4P - Conveyor tracking: path velocity of axis groups 'AxesGroup.lrPathVelocity' not unique (fixed as of V03.32.00)
Removed as…
URL:
/ru-ru/go/akb/202400060/1
Project compare: Usability improvement
Function extension:As of PLC Designer V4.0, the following usability improvement at project…
URL:
/ru-ru/go/akb/202500007/1
L_MC1P_Limiter and 'Safely limited speed' (SLS): Profile generation also incorrectly takes place below the limitation with the SLS delay…
URL:
/ru-ru/go/akb/202400059/1
Import PLCOpenXML: Usability improvement
Function extension:As of PLC Designer V4.0, the following usability improvement at import of…
URL:
/ru-ru/go/akb/202400055/1
Improvements at IEC 61131-3 Editors
Function extension:As of PLC Designer V4.0, the following improvements are now included in the…
URL:
/ru-ru/go/akb/202500055/1
New command: Edit IO mapping
Function-extension:The new context menu command 'Edit IO mapping' of the EtherCAT master opens an…
URL:
/ru-ru/go/akb/202400425/1
Partial access to bit string variables
Function-extension:Partial access to bitstring variables is performed with a similar syntax to…
URL:
/ru-ru/go/akb/202400422/1
Project Inspector
Function-extension:From PLC Designer V4.0, the project inspector checks which version the project was created with…
URL:
/ru-ru/go/akb/202300148/1
Symbolic access to the process image
Function extension: From PLC Designer V4.0, direct access to all IO channels of a device is now…
URL:
/ru-ru/go/akb/202500008/1
i750 with absolute encoder and position reconstruction: After replacing the device, the machine must be re-referenced (fixed from…