URL:
/sl-si/go/akb/20010093/1
Updating time of variables in DDS display
Question:
How fast can a variable be shown in the DDS display (monitored)?
Answer:…
URL:
/sl-si/go/akb/20010092/1
L_ParRead, L_ParWrite in the system POE 'PLC_ColdStart'
Question:
Why can some function blocks not be used in the system POE…
URL:
/sl-si/go/akb/20010090/1
Operating mode 'SSC' with 9300 Servo PLC (without feedback)
Question:
In the 9300 Servo PLC, is there an operating mode without a…
URL:
/sl-si/go/akb/20010087/1
Flag with temporary codes
Question:
Why are the temporary codes necessary?
Answer:
Temporary codes are flags connected to…
URL:
/sl-si/go/akb/20010086/1
L_Mpot, memory loss of the last value of the motor potentiometer (XXRetain input)
Question:
Why can the motor potentiometer L_Mpot…
URL:
/sl-si/go/akb/20010085/1
Triggering a further process by changing a code
Question:
How, when changing a code, is it possible to trigger a further process…
URL:
/sl-si/go/akb/20010084/1
Parameter manager (ServoPLC), type equivalent of instance name
Question:
What has to be done to make it possible to grant the same…
URL:
/sl-si/go/akb/20022305/1
GDC access to almost all codes is denied
Application
GDC is to be connected to a drive (with field bus communication).
Problem
When…
URL:
/sl-si/go/akb/20010055/1
Identifier area can be moved with the Free CAN objects
Question:
Why, when using the initialisation function 'L_CanInit' on the Free…
URL:
/sl-si/go/akb/20010041/1
GDC device description for Servo PLC with positioning library
Question:
Is there a separate device description (PDB) for Servo PLC…
URL:
/sl-si/go/akb/20010033/1
Parameterisation or programming, explanation of terms for controller 9300
Question:
What is the difference between parameterisation…
URL:
/sl-si/go/akb/20010029/1
Saving parameter sets in keypad 9371, which is activated in the drive controller after transfer?
Question:
Why, after saving all the…