URL:
/sl-si/go/akb/202000105/1
Troubleshooting "Ethernet based communication systems"
Questions:What should be done in the event of a communication fault in an…
URL:
/sl-si/go/akb/202500039/1
New menu command: Combine/Separate doubleaxis
Function-extension:With the new context menu command 'Combine doubleaxis', two selected…
URL:
/sl-si/go/akb/202400247/1
Language selection is not up-to-date in the Settings dialog if language was added in EASY UI Designer
Corrected from:Behavior of the…
URL:
/sl-si/go/akb/202500180/1
Add additional languages
Question:How can I add a language to the EASY UI Designer that cannot be added via the Project…
URL:
/sl-si/go/akb/202400246/1
Designer: Target device selection dialog does not match project settings
Corrected from:EASY UI Designer V1.5Behavior of the new…
URL:
/sl-si/go/akb/202300515/1
Design Time: The EASY UI Designer will be closed with an exception when the connected controller is restarted via "0x2022:035" in PLC…
URL:
/sl-si/go/akb/202300516/1
Runtime - Language: The fallback language is partially not displayed
Corrected from:behavior of the new version:Description of…
URL:
/sl-si/go/akb/202500176/1
PLC Designer: Unexpected request for Download of application
Corrected from:Behavior of the new version: Description of the…
URL:
/sl-si/go/akb/202500122/1
Error message 'Root element missing' when starting the EASY Package Manager
Corrected from:EASY Package Manager V1.28Behavior of the…
URL:
/sl-si/go/akb/202500127/1
OPC UA - Data type change of the diagnostics parameter "Active Setting" (with old PLC Designer project and new firmware)
Compatibility…
URL:
/sl-si/go/akb/202300466/1
OPC UA client / security: encrypted communication with the exchange of certificates
Function extension: This firmware version…
URL:
/sl-si/go/akb/202400148/1
Data access from OPC UA to the logic is not synchronised with the PLC cycle
Question:Does OPC UA read the data at the beginning and…