URL:
/sl-si/go/akb/20010382/1
Field weakening, reduction of the maximum torque
Question:
What can be the reason that in case of vector control the drive does not…
URL:
/sl-si/go/akb/20010337/1
Monitoring setting for DDS
Question:
Can the monitoring window in the DDS be set individually in order to monitor variables and…
URL:
/sl-si/go/akb/20010314/1
Components of the DDS project documentation
Question:
Which components are necessary for complete project documentation?…
URL:
/sl-si/go/akb/20010177/1
Restart after short mains disconnection
Question:
Why does a short mains disconnection (8200vector) cause a restart after resumption…
URL:
/sl-si/go/akb/20010176/1
NTC making current limiting, application for 400 V three-phase network
Question:
Are the NTC making current limits (250 V) also…
URL:
/sl-si/go/akb/20020999/1
OC1 or OU-TRIP during activation of GSB at high rotary speeds
Question:
What can be the cause of OC1- or OU-TRIP if the DC brake is…
URL:
/sl-si/go/akb/20023928/1
Oil change interval
Question:
Which oil change intervals have to be observed with the gearbox?
Answer:
Gearboxes in frame…
URL:
/sl-si/go/akb/20020717/1
Function comparison GDC with GDCeasy
Question:
What are the differences between GDC and GDCeasy?
Answer:
GDCeasy offers the…
URL:
/sl-si/go/akb/20020627/1
HMI Designer - wrong file name in the box title
Question:
Why in HMI Designer is a wrong file name shown in the window title of the…
URL:
/sl-si/go/akb/20020624/1
Can 120 ohm bus terminating resistor be switched off?
Question:
When using system module 2173IB with the associated system cable a…
URL:
/sl-si/go/akb/20020549/1
Position limits cannot be reached
Question:
What could be the reason for the fact that that the drive cannot be positioned up to the…
URL:
/sl-si/go/akb/20020518/1
Resetting the integrated process controller
Question:
How can a process controller reset be performed?
Answer:
A reset of…
URL:
/sl-si/go/akb/20020492/1
Cam number at CDATA-ACTCAM
Question:
Which cam number is indicated at CDAT-ACTCAM?
Answer:
First of all CDATA-ACTCAM has to…
URL:
/sl-si/go/akb/20020491/1
CDATA-XACT, CDATA-XPOS - functional description of the output signals
Question:
How do CDATA-XPOS and CDATA-XACT relate to one…