Factory reset a device

Factory resetting a device (x500) will return all settings on the device to their factory default value. You cannot undo a factory reset! After doing a factory reset you’ll have to register the device again. If the device is still listed in X4 Remote and you want to re-use those settings, make sure to turn on “Recover upon next registration” before registering again. If you want to start from scratch, make sure to remove the device from X4 Remote before registering again.

Factory reset a device

Remove USB and use stable power
Make sure the power supply is stable, as losing power during a factory reset will result in a defective unit. Also make sure to remove the USB flash drive from the device, if one is present.

Carefully follow the steps below to factory reset your device.

  • On top of the device, near the back, you’ll see a small round opening. Grab a pencil or other pointy object and gently press and hold the factory reset button inside the opening.

After a few seconds, the LEDs on the device should start flashing, indicating that it is busy performing the factory reset.

  • Keep holding the button until the LEDs stop flashing and then let go.

The ACT LED should now be constant red.

  • Wait 2 minutes.

The device will now boot up. If after 2 minutes the ACT LED is still constant red, that means the factory reset was executed correctly. If it is not constant red, that means you likely let go of the factory reset button too early and you’ll need to repeat the steps above.

After a factory reset
If the device is still listed in X4 Remote and you want to re-use those settings, make sure to turn on "Recover upon next registration" before registering again. If you want to start from scratch, make sure to remove the device from X4 Remote before registering again.

 

Yhteystiedot