Modbus TCP/IP
Supported hardware and firmware
Cloud Notify via Modbus TCP/IP is supported on the x500 in firmware 3.7 and up. Please upgrade your firmware if you are running an older version.
Activate Cloud Notify
Please first activate Cloud Notify (or start the 30 day free trial) if you haven't already.
The Second step in Cloud Notify is setting up a data source. This is done by selecting a communication protocol and defining the variables. This article shows you how to do this for communication via Modbus TCP/IP.
- Select a communication protocol
- Add variables
- Test variables
- Manage variables
Select a communication protocol
You first have to select a communication protocol. This is the protocol that the x500 will use to communicate with the PLC.
- Go to the Fleet Manager app, which is accessible from the Apps menu in the top right corner if you are currently in a different X4 Remote app.
- Open the Main menu, go to Devices, and select the concerning device.
- Click on the Add a service icon in the left menu, select [Data source], and then select [Modbus].
- Enter the requested information (details below) and click on [Add].
Field | Description |
---|---|
Name | Enter a name for the data source. |
Identifier | The identifier ensures that every data source remains unique, even if they share the same name. |
IP address | Enter the IP address of your PLC. |
Port | The port number will be entered automatically (Port 502 for Modbus). |
Slave & Byte order | Enter the Modbus server’s slave ID and byte order. The byte order determines how the bytes in a register are translated to a numerical value. |
Polling sleep time | To log data as accurately as possible, the x500 continuously asks the variables’ values from the PLC (this does not count towards your license’s dps/hr). While the x500 does wait for the PLC to reply before asking again, in very rare cases this may noticeably impact the PLC’s performance. In such a rare situation you may want to change this setting to 100ms or higher. In general “None” is recommended for Cloud Logging to be as accurately as possible. |
Add variables
Once you’ve added a data source and selected a communication protocol, you can start adding variables. You can do this by following the steps below:
- Expand the Data source service and go to [Variables].
- You can now choose to:
- Manually add new variables
- Import variables from a file (or device)
Tip!
It is advisable to add variables in small batches and test them to verify their configuration.
Manually add new variables
- Click on [Add variable] in the bottom right corner.
- Enter the requested information (details below) and click on [Add].
Field | Description |
---|---|
Name | Enter a name for the variable. |
Identifier | The identifier ensures that every variable remains unique, even if they share the same name. |
Type | Select the variable’s data type (bool, int, float, etc). |
Function Code | Enter the variable’s function code (details below). |
Address | Enter the variable’s address (details below). |
Factor | Multiplies the value (leave empty if the data type is boolean). |
Unit | Displayed text behind the value. |
Modbus explained - number vs address
A Modbus number translates to a function code with an address, and vice versa. Depending on your program you will know one of the two notations. Use the following example table for help with translating between the two. "Number" notation "Address" notation Number Function code Address 000011 1 - Coil 10 100381 2 - Discrete input 380 400093 3 - Holding register 92 300135 4 - Input register 134
Temporary disconnect
After this next step, the config push, the device may temporarily disconnect and LAN communication may be temporarily interrupted while it's applying the new settings. This may take a minute.
You have now made the changes in X4 Remote, but these are not yet active in your device. You will need to push your changes to your device for them to take effect.
- Click [Push config to device] in the top right corner.
Next step
Now that you've added the variables, you can test if they're configured properly.
Import variables from a file (or device)
You can easily and effortlessly copy variables from one device to another by exporting the concerning variables (view the “Manage variables” part of this article) and then importing them in your new device. Alternatively, you can manually prepare your variables in the required CSV format to load them all at once into your configurator. The CSV file structure is explained in our Import variables article.
- Click on [Import from CSV-file] in the top right corner of the screen.
- Select a CSV file to import and click on [Open].
Temporary disconnect
After this next step, the config push, the device may temporarily disconnect and LAN communication may be temporarily interrupted while it's applying the new settings. This may take a minute.
You have now made the changes in X4 Remote, but these are not yet active in your device. You will need to push your changes to your device for them to take effect.
- Click [Push config to device] in the top right corner.
Next step
Now that you've added the variables, you can test if they're configured properly.
Test variables
The test utility is used to check if all the added variables are set correctly. It shows the communication status with the PLC and displays each variable’s current value if everything is configured correctly. If not, the values will stay empty. The test utility will attempt to update values every 0.5 seconds, regardless of how often it’s actually being logged (this does not count towards your license’s dps/hr). Please follow the steps below to test your variables.
- Expand the Data source service, go to [Variables], and click on [Run test] at the top.
A connection will now be set up to stream the data directly to your computer, using:
Port | Transport protocol | Application protocol |
---|---|---|
443 | TCP | WebSocket |
You will see live values of all variables, if the configuration is set up correctly.
Unexpected result?
If the test utility shows unexpected values, please check if the addresses and data types of all variables are entered correctly. If you get an error message, please check Common error messages for more info. If you get no data at all, please also check that the above listed port and protocols are not being blocked by your computer's or company's firewall.
Next step
Now that you've tested the variables, you can view our "Configure data tags" guide to start logging.
Manage variables
You can view all defined variables on the variables page:
- Expand the Data source service and go to [Variables].
You can [Edit] individual variables, [Remove] individual or a selection of variables, and export all or a selection of variables.
Variables can be selected by clicking the checkbox on the left, or you can select them all by clicking the checkbox at the top.