URL:
/tr-tr/go/akb/20024077/1
I²xt function of the 8200 vector / motec
Question:
How are parameters set to the internal motor temperature monitoring (I²x t…
URL:
/tr-tr/go/akb/20024186/1
Register mark or cylinder mark distance, standardisation
Question:
Which value does the standardisation of the following code digits…
URL:
/tr-tr/go/akb/20024298/1
Current controller adjustment, setting the current controller parameters (C0075, C0076), 9300 and ECS
Question:
Under which…
URL:
/tr-tr/go/akb/20024333/1
Text panels, input of special characters and umlauts
Question:
How can special characters or umlauts are entered in text panels H…
URL:
/tr-tr/go/akb/20024334/1
Detection of task run times for further calculations in the PLC
Question:
How can the run time of the current task be detected?…
URL:
/tr-tr/go/akb/20024346/1
DFSET stretch factor and gearbox factor, correct order
Question:
What has to be considered for the use of stretch factor and gearbox…
URL:
/tr-tr/go/akb/20011608/1
Synchronous motor applied to frequency inverter
Question:
Can a synchronous motor (e. g. SDSGS synchronous servomotor) be applied to…
URL:
/tr-tr/go/akb/20011602/1
Armature chokes, typical temperature during operation of armature chokes
Question:
Which typical surface temperatures are normal /…
URL:
/tr-tr/go/akb/20011537/1
Mains voltage, adaptation C0173
Question:
Which influence does the adaptation have on the mains voltage threshold via code digit…
URL:
/tr-tr/go/akb/20022318/1
Group drive, input of motor data in vector control and V/f-characteristic
The motors, which are connected in parallel at the output of the…
URL:
/tr-tr/go/akb/20030639/1
Parallel operation of breaking units 9350, maximum number of devices
Question:
How many breaking units can be operated at the same…
URL:
/tr-tr/go/akb/20011471/1
Motor temperature monitoring with early warning
Question:
Which settings are to be done, so that in case of motor overheat first,…
URL:
/tr-tr/go/akb/20011455/1
Oscilloscope in the GDC: Is a signal overrun possible?
Question:
Can signals, which are shown in the GDC internal oscilloscope,…
URL:
/tr-tr/go/akb/20011446/1
LEMOC2, operating systems MSDOS and Microsoft Windows
Question:
LEMOC2 can be applied to which operating system?
Answer:
LEMOC…