URL:
/sk-sk/go/akb/20022969/1
Mains supply conditions, voltage levels, automatic mains detection, ECS supply module
Question:
How does the automatic mains…
URL:
/sk-sk/go/akb/20023018/1
Feedback not at the motor shaft, odd-numbered ratio
Question:
How can an incremental encoder be used as speed feedback, if it is not…
URL:
/sk-sk/go/akb/20011354/1
Motor parameter identification, warm or cold motor?
Question:
Is the motor identification (ID run, this means C0148 = 1) in the…
URL:
/sk-sk/go/akb/20023044/1
Profibus address assignment without parameter setting via keypad or GDC
Question:
How can the profibus station address be assigned…
URL:
/sk-sk/go/akb/20023058/1
Torque M0 in case of continuous operation S1, which meaning does it have?
Question:
Why an increasing torque of asynchronous motors…
URL:
/sk-sk/go/akb/20023060/1
Register mark, automatic window adjustment
Question:
How is the automatic window adjustment realised for a register mark?…
URL:
/sk-sk/go/akb/20023081/1
Switch-on inhibit, LOCK-MODE
Question:
What does the display switch-on inhibit (LOCK-MODE) in the display of the keypad or in the…
URL:
/sk-sk/go/akb/20023190/1
Graphic operator-controllable by touch areas
Question:
How can a graphic (BMP, JPG,...) be made operator-controllable by touch areas…
URL:
/sk-sk/go/akb/20023196/1
Define fonts in HMI Designer Projects
Question:
Which define fonts are offered by the HMI Designer for generation of display pages?…
URL:
/sk-sk/go/akb/20023213/1
Acceleration delay after pulse inhibit due to active earth fault detection
Question:
Why is there an acceleration delay after pulse…
URL:
/sk-sk/go/akb/20023204/1
U15 - What does this fault indication mean?
Question:
What does the fault indication U15 mean in case of 9300 controllers?…
URL:
/sk-sk/go/akb/20023284/1
Touch Probe residual distance, positioning direction
Question:
How is the touch probe residual distance processed after the touch…
URL:
/sk-sk/go/akb/20024357/1
Logic operations: Possibilities for the optimisation of logic interconnections
Question:
How can complicated logic operations (AND,…
URL:
/sk-sk/go/akb/20023290/1
V-override, drive performance when V-override = 0 %, S-ramps
Question:
Why does the positioning drive still move with low speed,…
URL:
/sk-sk/go/akb/20023294/1
S-ramps, code C1257 (PARAM-RD-filter)
Question:
What effect does the input under code C1257 have?
Answer:
The code C1257 has…