Lenze Whitepaper
Plug & Produce for the Smart Factory
Lenze Knowledge #9
Self-managing production lines are here! In the flexible production of the future, machine modules will not only be coupled automatically, they will coordinate themselves as part of a production line, communicate and interact in the production process. With the Plug & Produce concept, Lenze presents the path into this future. Plug & Produce is an open, flexible and manufacturer-independent communication and integration concept for machines and production lines, based on the OPC UA communication standard using the “administration shell” for machine description as well as their capabilities ("skills"). The white paper describes the concept of Plug & Produce, what is already possible today and which steps are necessary for successful implementation.


Cross-machine communication
Lenze Knowledge #8
The whitepaper OMAC PackML provides an insight into the topic of cross-machine communication based on standardized information models (PackML). It explains what lies behind the term PackML and how the standard is structured, but above all it focuses on the benefit argumentation from the user's point of view. Real examples from Procter & Gamble, Velux and Arla Foods show the advantages of using PackML from the end user's point of view. The examples of Mettler Toledo and the ProMach Group illustrate how machine manufacturers also benefit from the use of PackML. The mentioned references and testimonials can be used in daily sales work.
Business Models for Industry 4.0
Lenze Knowledge #7
As digitalization progresses, new doors are constantly opening to customers, processes and data that were previously closed, or at least could not be used economically until now. Who doesn't dream of the disruptive business model with which the market is conquered and which leaves the competition left behind astonished.
But it's not that simple. A good portion of luck is needed to get there. In addition, success is based on a combination of a fundamental understanding of the success factors of innovation, organizational skills and hard, small-scale work, which places learning progress in the foreground and not the achievement of target figures. This whitepaper establishes the relation between these topics and brings the hyped topic "new business models" back to the ground of mechanical engineering reality.


L'Industrie 4.0 parle OPC UA
Connaissance Lenze #6
La technologie OPC UA est devenue incontournable pour les fabricants de machines, les intégrateurs systèmes et les utilisateurs qui souhaitent être à la pointe de l'Industrie 4.0. Ils doivent se familiariser au plus vite avec les capacités et les fonctionnalités de cette technologie d'interopérabilité et réfléchir sérieusement et de manière critique à son intégration dans leurs propres systèmes.
Mais qu'y a-t-il derrière ? D'où cela vient-il ? Et à quoi cela sert-il ?
Le Livre Blanc répond à ces questions et explique également pourquoi OPC UA est plus qu'un simple système de bus de terrain.
Le jumeau numérique
Connaissance Lenze #5
Les fabricants de machines sont constamment soumis à des contraintes de temps et de coûts. Respecter les délais de livraison, ne pas perdre de vue les spécifications convenues et procéder aux ajustements du logiciel lors de la mise en service pendant qu’on a le client sur le dos. En cas de problème, il peut arriver rapidement que plusieurs essais soient nécessaires avant que le prototype ne corresponde pleinement aux exigences du client. Et lorsque cela arrive, le calcul des coûts est déjà une perte de temps. L'ingénierie numérique permet de sortir de ce dilemme.
Aujourd'hui, une grande variété d'outils logiciels extrêmement pointus est déjà utilisée pour développer, simuler, vendre ou gérer des machines. Cependant, bon nombre des solutions disponibles sont encore des solutions isolées et il n'existe pas de chaîne de processus numérique continue dans de nombreux domaines. Ce Livre Blanc accompagne un robot tout au long du cycle de vie d'un produit et utilise différents exemples pour expliquer la vision derrière le jumeau numérique et tous les avantages qu'il nous promet dans des phases très différentes.

Cloud computing dans l'ingénierie mécanique
Connaissance Lenze #4
Dans le cadre de la transformation numérique, le Cloud Computing est sur toutes les lèvres – mais de quoi s'agit-il exactement et comment un équipementier peut-il en tirer profit ?
Ce livre blanc fournit des connaissances de base détaillées sur le cloud computing et les modèles de services associés. Il présente les avantages et montre comment simplifier le déploiement. Le livre traite des risques et des obstacles auxquels les utilisateurs du cloud peuvent être confrontés, aide à choisir le bon modèle de cloud computing et détaille les différentes méthodes de facturation. La représentation orientée application du cloud dans le processus de production est essentielle. Des exemples pratiques montrent comment le cloud permet de faire des progrès concrets grâce à l'analyse et au traitement des données.
Le dilemme des logiciels dans la construction de machines et d'installations
Connaissance Lenze #3
La digitalisation est en train de changer radicalement l'ingénierie mécanique. La complexité des machines et le degré de personnalisation augmentent et de nouveaux services et modèles économiques se développent. Par conséquent, l'effort financier pour les logiciels s'accroît de façon exponentielle. Il faut donc trouver les moyens de rendre la programmation plus efficace.
Cependant, un savoir-faire technique supplémentaire n'est pas la seule réponse. Pour bénéficier des méthodes de développement modernes, l'organisation des processus doit également changer chez les équipementiers. Ce livre blanc explique en termes pratiques quels aspects de la situation actuelle posent problème et répond à la question de savoir comment l'ingénierie mécanique peut encore se développer. L'accent est mis sur l'adaptation plus rapide des machines aux exigences des clients ainsi que sur la conception plus efficace des processus de développement par des méthodes agiles et sur la question de l'assurance qualité cohérente dans le développement logiciel.
Sécurité fonctionnelle
Connaissance Lenze #2
La réglementation européenne sur la sécurité des machines, appelée Directive Machines 2006/42/CE, stipule que le constructeur doit garantir la sécurité des personnes, des machines et de l'environnement tout au long du cycle de vie (et dans tous les modes de fonctionnement). Le fabricant assume la responsabilité de la conception et de la fabrication de sa machine. Après avoir suivi des procédures de vérification, il doit attester que sa machine est conforme aux exigences de sécurité en apposant un marquage CE. Et si, un accident survient du fait d'un défaut de conception de sécurité, c'est le chef d'entreprise qui est responsable à titre personnel.
De nombreuses obligations sont à remplir afin d'éviter d'en arriver à ce cas extrême. Des exigences de sécurité sont énoncées dans d'innombrables lois et directives. Ce livre blanc donne un aperçu des exigences légales, des conseils sur la mise en œuvre et des conséquences de la non-conformité. Le document traite également de l'interaction entre la sûreté et la sécurité. Alors que, dans le passé, les deux sujets étaient souvent perçus comme opposés, la sécurité et la sûreté sont maintenant devenues des enjeux communs qui doivent être considérés et traités ensemble. Ce livre traite également des possibilités ouvertes par la sécurité fonctionnelle. Trois exemples concrets montrent comment la sécurité est directement profitable. Ceux qui souhaitent approfondir le sujet trouveront également une liste intéressante de références bibliographiques qui, en plus des normes et des directives, comprend en particulier des documents d'interprétation importants.
Le défi du numérique
Connaissance Lenze #1
Notre premier livre blanc décrit de façon pragmatique les étapes à suivre pour maîtriser la transformation numérique. Il aborde aussi le fait que le passage du développement de produits classiques à la gestion de l'innovation nécessite des ajustements de la structure et de la culture de l'entreprise. Enfin, il est complété par des connaissances de base et la classification des divers environnements, des conseils pour surmonter les obstacles et des suggestions de lectures complémentaires.
Ce livre blanc s'adresse en premier lieu aux chefs d'entreprise et aux responsables du management.