Plug & Produce for the Smart Factory

Lenze Knowledge #9

Self-managing production lines are here! In the flexible production of the future, machine modules will not only be coupled automatically, they will coordinate themselves as part of a production line, communicate and interact in the production process. With the Plug & Produce concept, Lenze presents the path into this future. Plug & Produce is an open, flexible and manufacturer-independent communication and integration concept for machines and production lines, based on the OPC UA communication standard using the “administration shell” for machine description as well as their capabilities ("skills"). The white paper describes the concept of Plug & Produce, what is already possible today and which steps are necessary for successful implementation.

Download Whitepaper

Cross-machine communication

Lenze Knowledge #8

The whitepaper OMAC PackML provides an insight into the topic of cross-machine communication based on standardized information models (PackML). It explains what lies behind the term PackML and how the standard is structured, but above all it focuses on the benefit argumentation from the user's point of view. Real examples from Procter & Gamble, Velux and Arla Foods show the advantages of using PackML from the end user's point of view. The examples of Mettler Toledo and the ProMach Group illustrate how machine manufacturers also benefit from the use of PackML. The mentioned references and testimonials can be used in daily sales work.

Download Whitepaper

Business Models for Industry 4.0

Lenze Knowledge #7

As digitalization progresses, new doors are constantly opening to customers, processes and data that were previously closed, or at least could not be used economically until now. Who doesn't dream of the disruptive business model with which the market is conquered and which leaves the competition left behind astonished.

But it's not that simple. A good portion of luck is needed to get there. In addition, success is based on a combination of a fundamental understanding of the success factors of innovation, organizational skills and hard, small-scale work, which places learning progress in the foreground and not the achievement of target figures. This whitepaper establishes the relation between these topics and brings the hyped topic "new business models" back to the ground of mechanical engineering reality.

Download Whitepaper

La industria 4.0 habla OPC UA

Lenze Knowledge #6

No existe ningún tema de la industria 4.0 sin comunicación, ya que todo –dispositivos, módulos y máquinas– se comunica en todas las direcciones. Y siempre se oye hablar de OPC UA.

Pero ¿qué es eso? ¿De dónde viene? ¿Y para qué sirve?

El Whitepaper responde a estas preguntas y también explica por qué OPC UA es más que un sistema de bus de campo cualquiera.

Descargar Whitepaper

El gemelo digital

Lenze Knowledge #5

La construcción de máquinas está bajo una presión constante en cuanto al tiempo y los costes: cumplir plazos de entrega, no perder de vista las especificaciones acordadas y realizar adaptaciones del software durante la puesta en marcha con uno de los clientes vigilando de cerca. Cuando surgen problemas, es muy fácil que se requieran varios intentos hasta que el prototipo cumpla completamente los requisitos del cliente. Pero entonces el cálculo de costes ya no sirve de nada. Una solución para este dilema es la ingeniería digital.

Hoy en día ya se utilizan herramientas de software muy variadas y altamente especializadas para desarrollar, simular, vender y gestionar máquinas. No obstante, muchas de las soluciones disponibles constituyen aún soluciones aisladas y en muchos puntos falta una cadena de procesos digital uniforme. El Whitepaper acompaña a un robot por todo el ciclo de vida del producto y, con ayuda de diferentes ejemplos, explica la visión que se esconde tras el gemelo digital y qué beneficios promete este en las tan diferentes fases.

Descargar Whitepaper

Cloud Computing en la construcción de máquinas

Lenze Knowledge #4

Como parte de la transformación digital, el Cloud Computing está en boca de todos, pero ¿qué es exactamente y cómo pueden los OEM beneficiarse de él?

El Whitepaper ofrece información fundamental detallada sobre el Cloud Computing y los modelos de servicio vinculados a él. Explica sus ventajas y muestra cómo puede facilitar la configuración. El documento está dedicado a los riesgos y obstáculos que se pueden encontrar los usuarios de la nube, ayuda a elegir el modelo de nube adecuado y explica los diferentes métodos de facturación. En este sentido, la representación cercana a la aplicación de la nube en el proceso de producción es esencial. Se presentan ejemplos prácticos sobre los avances concretos que ofrece la nube mediante análisis y tratamiento de datos.

Descargar Whitepaper

Dilema del software en la construcción de máquinas

Lenze Knowledge #3

El mundo digitalizado cambiará la construcción de máquinas para siempre. La complejidad de las máquinas y el grado de personalización aumentan. Además, se desarrollan nuevos servicios y modelos de negocio. En consecuencia, el trabajo se software aumenta exponencialmente. Por eso se deben encontrar medios y recursos para hacer que la programación sea más efectiva.

Solo con un know-how especializado adicional no basta. Para poder beneficiarse de los métodos de desarrollo modernos, los OEM deben cambiar también la organización de los procesos. El Whitepaper explica de manera práctica qué aspectos del statu quo plantean problemas y responde a la pregunta de cómo puede seguirse perfeccionando la construcción de máquinas. La adaptación más rápida de las máquinas a los requisitos de los clientes también constituye el centro de atención, así como el diseño más eficiente de los procesos de desarrollo mediante métodos ágiles y la demanda de una garantía de seguridad consecuente del desarrollo de software.

Descargar Whitepaper

Seguridad funcional

Lenze Knowledge #2

Los reglamentos sobre seguridad de las máquinas establecen que el fabricante de una máquina debe garantizar la seguridad de las personas, las máquinas y el medio ambiente durante todo el ciclo de vida (y en todos los modos de operación) de la máquina. Si la dirección no cumple estos requisitos, deberá responsabilizarse de las consecuencias, en algunos casos incluso con su patrimonio privado.

Se deben cumplir muchas obligaciones, que están documentadas en incontables leyes y directivas. El Whitepaper ofrece un resumen de los requisitos jurídicos, consejos de implementación y las consecuencias del incumplimiento. Otro punto que se trata es la interacción entre Safety y Security. Mientras que estos dos temas se habían considerado como contrarios en el pasado, ahora están estrechamente relacionados y se deben tener en cuenta y tratar juntos. El documento también trata las oportunidades que ofrece la seguridad funcional. Con tres ejemplos concretos se demuestra cómo la seguridad vale la pena. Los que quieran profundizar en la materia encontrarán una bibliografía interesante que, además de normas y directivas, incluye particularmente documentos interpretativos importantes.

Descargar Whitepaper

El desafío digital

Lenze Knowledge #1

Nuestro primer Whitepaper muestra de una forma pragmática los pasos que debe tomar para dominar la digitalización, y es que el camino desde el desarrollo de productos clásico hasta la gestión de la innovación también requiere cambios en la estructura y la cultura de la empresa. El documento se complementa con conocimientos básicos y la clasificación de contextos, consejos para superar obstáculos y propuestas para seguir leyendo.

El Whitepaper está dirigido principalmente a gerentes y responsables de la administración de empresas.

Descargar Whitepaper