Plug & Produce: Smart Factory Soon a Reality

Plug & Produce uses Industry 4.0 concepts and digital transformation to generate concrete, measurable benefits.

Greater individualisation, smaller batch sizes, more frequent configuration changes, but with cost-efficient and competitive production lines - a contradiction? A huge challenge in any case. The Plug & Produce concept could soon mean that the production line is back in operation without excessive engineering effort being required for configuration and programming. Interfaces standardised across manufacturers for control, configuration, and product data already exist. With the concept of administration shells and machine skills, Lenze demonstrates what the future could look like. Visitors can experience Industry 4.0 live from 1st to 5th April at the Hannover Messe at the Lenze stand in Hall 14, H22.

Mechanical engineers and plant operators are asking what the concrete, measurable benefits of Industry 4.0 and the digital transformation are. With its real-world showcase, Lenze, the specialist for machine automation,demonstrates how this "digital dividend" can be leveraged. Plug & Produce is an application which combines the various elements of Industry 4.0 and enables progress to be made where the efficiency of modern production is concerned.

The showcase simulates the packaging of various consumer products - such as washing detergent and creams - with different modules in a production line. The retrofitting of the production line follows the "Plug & Produce" concept - plug in and get started. The key idea revolves around how a production line can easily be adapted to changing requirements without a significant loss in production.

Customised production lines
The starting position for the showcase is a modularisation of the production line. The individual modules - including Infeed, Pick & Place, Packaging, Palletiser and Outfeed - represent the required elements which are made available to production. The process required for packaging creams differs from those for the packaging of washing detergents.

If the corresponding modules of the production line are replaced, the control system will need to be reprogrammed. With the Plug & Produce approach, this is far easier and quicker. The line is reconfigured in a moderation phase. This takes place via the uploading of configurations which now do not just control the manufacturing process itself, but also contain information on which tasks are to be performed in which sequence, such that the modules can be selected and linked.

The modules themselves provide the information, for example, the height at which transfer points such as a conveyor belt are located, at which position workpieces are to be delivered or how they are fed out and at what speed they can be processed. If the plausibility check shows that all the required processes are available, at the right position, and with the appropriate physical interfaces, the production phase can start.

Focus on the digital description of the modules
The next step towards the smart factory is based on the administration shell, which was adopted as part of the reference architectural model Industry 4.0 (RAMI 4.0) in April 2018. There can be administration shells not just for individual components, but also modules or the entire machine. The data they contain provide information on the physics - such as connecting dimensions, service life, operation values - and on the process: is it a drive, a network component, a packaging module, or a welding installation? This data forms the basis for creating a digital twin which allows programming and simulation to take place long before the physical implementation of a machine.

The secret lies in communication: open, manufacturer-independent standards allow the various modules and the PLC involved to automatically exchange administration shell data with each other, or even engage in full-fledged interaction during production. For this purpose, a unified data and information model as well as standardised semantics are required so that the data can also be interpreted correctly. The first part of these preconditions is fulfilled by the administration shell. For the second part, Lenze utilises an expansion of the information and communication platform OPC UA. In fact, the OPC UA Companion Specification PackML served as the basis for its own showcase.

The right path towards the future
In order for this concept to function not just in Lenze's own showcase, but also in mixed environments in the field, a certain amount of homework still needs to be done. The main prerequisite is that all current components for mechanical engineering and automation are outfitted with an administration shell by the manufacturer. Secondly, there is still a gap that needs to be closed where standardisation is concerned. Lenze is active on numerous committees in this regard, always with the aim of reaching a manufacturer-neutral, open solution. Once this step has been completed successfully, the developer tools will need to be further developed such that they are able to interpret and utilise the data which accumulates across the various lifecycle stages in the administration shell of components and machines.

OEMs should already gear themselves towards this development, which will manifest as part of digital engineering. Above all, modularisation will need to be emphasised when creating the control software. This allows the machine builder to benefit from Plug & Produce as well, allowing a faster time-tomarket to be realised with the use of fewer resources. The manufacturer from Hamelin is already offering comprehensive consulting services for this purpose, thereby providing guidance and paving the way for those who wish to make progress where Industry 4.0 is concerned.

Contact form